HRB1684301-17

Alarm/energy pulsing LED

The alarm/energy pulsing LED can be configured for alarm notification or energy pulsing.

When configured for alarm notification, this LED flashes when a high, medium, or low priority alarm is active indicating an active alarm condition or an inactive but unacknowledged high priority alarm.

When configured for energy pulsing, this LED flashes at a rate proportional to the energy consumption which is typically used to verify the power meter’s accuracy.

The alarm/energy pulsing LED on the MID/MIR models is permanently set for energy pulsing and cannot be disabled or used for alarms.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?