HRB1684301-12

Binary Input objects

Your meter has a number of Binary Input objects that provide the status information from the meter’s I/O.

The following table lists the Binary Input (BI) objects available on the meter.

Object ID Object name Description
38416 – 38419

Digital Input 1

Digital Input 2

Digital Input 3*

Digital Input 4*

Status of digital inputs:

  • 0 = on
  • 1 = off

NOTE: This information only applies if the digital input is configured as a status input.
38448, 38449

Digital Output 1

Digital Output 2

Status of digital outputs:

  • 0 = on
  • 1 = off

*Available in specific meter models. Refer to Features differentiation matrix for PM5500 / PM5600 / PM5700 series for the availability.

QR code for this page

Was this helpful?