HRB1684301-15

Configuring DNP3 setting using the display

The Ethernet setup screen on the meter allows you to configure DNP3 communication.
  1. Navigate to Maint > Setup .
  2. Enter the setup passcode (default is “0”), then press OK.
  3. Navigate to Comm > Enet .
  4. Move the cursor to point to the parameter DNP3 you want to modify, then press Edit.
  5. Modify the parameter as required (Enabled/Disabled), then press OK.
  6. Press the up arrow to exit.
  7. Press Yes to save your changes.
QR code for this page

Was this helpful?