HRB1684301-15

Default data display screen

The default data display screen varies depending on the meter model.

The Summary screen is the default screen for all meter models except PM5561 / PM5661 / PM5761 .

The Summary screen displays real-time values for average voltage and current (Vavg, Iavg), total power (Ptot) and energy consumption (E Del).

The Power System screen is the default screen for PM5561 / PM5661 / PM5761 meter models.

  A Accumulated real energy (delivered + received)
  B System frequency
  C Active tariff
  D Power system setting
  E Control power (auxiliary power) interruption event icon
  F Locked / unlocked icon
     

QR code for this page

Was this helpful?