Default passwords/passcodes and user accounts
Configuration area |
Username |
Default password/passcode |
|
---|---|---|---|
Display passcode |
— |
0000 (zero) |
|
For firmware versions:
|
Webpages and FTP
|
user1 user2 |
pass1 pass2 |
For firmware versions:
|
Webpages and FTP/FTPS |
Administrator |
MAC address which is unique for each meter NOTE: Enter the MAC address of the meter
without colon in capital letters (For example: if the MAC address
of the meter is 00:80:f4:02:14:38, then password is 0080F4021438).
NOTE: Forced to change the default password for system security the
first time you log in.
|
Webpages |
Guest |
Powerlogic@1 NOTE: Recommended to change
the default password for system security the first time you log in.
|