HRB1684301-12

Demand measurements

The meter provides present, last, predicted and peak (maximum) demand, and a date/timestamp when the peak demand occurred.

The meter supports standard demand calculation methods, including sliding block, fixed block, rolling block, thermal and synchronized.

Peak demand registers can be reset manually (passcode protected) or logged and reset automatically on a programmed schedule.

Demand measurements include:

  • kW, kVAR, kVA demand total and per phase

  • Amps demand average, per phase and neutral (4th CT)

  • Demand calculation for pulse input metering (WAGES)

QR code for this page

Was this helpful?