HRB1684301-16

Digital inputs

The meter is equipped with four digital inputs (S1 to S4) or two digital inputs (S1 & S2)*.

NOTE: *Available in specific meter models. Refer to Features differentiation matrix for PM5500 / PM5600 / PM5700 series for the availability.

You can configure the digital inputs for use in status monitoring or input metering applications.

The meter’s digital inputs require an external voltage source to detect the digital input’s on/off state. The meter detects an on state if the external voltage appearing at the digital input is within its operating range.

Refer to Device specifications for the external voltage sources to detect the digital input’s on/off state.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?