HRB1684301-12

Digital output application example

You can connect one of your meter’s digital outputs to a relay that switches on a generator and the other digital output to send a demand sync pulse to other meters.

In the following example, the first meter (Meter 1) controls and sets the demand period (900 seconds) of the other meters (Meter 2, Meter 3, Meter 4) through the output pulse occurring at the end of the first meter’s demand interval.

A Relay
B Demand period (in this example, 900 seconds)
   
QR code for this page

Was this helpful?