HRB1684301-15

Enabling and disabling the FTP server using the webpages

NOTE: Refer to Restoration of temporarily disabled configuration settings in webpages to know availability of these features on your meter model.

The FTP server on the meter needs to be enabled for certain meter functionality.

NOTE: The FTP server is Disabled by default for security reasons. You can Enable the FTP server, if required. It is recommended to use encrypted FTP (FTPS).
  1. Login to the meter webpages.
  2. Based on your meter firmware version, click Settings > Advanced Ethernet Settings OR click Settings > Communication > Advanced Ethernet Settings .
  3. Set FTP Server to Enabled or Disabled.
  4. Click Save Changes or Apply Changes to save your changes to the meter.
QR code for this page

Was this helpful?