HRB1684301-15

HMI setup screens

You can configure the meter’s display using the HMI setup screens.

The HMI (human-machine interface) setup screens allow you to:

  • control the general appearance and behavior of the display screens,

  • change the regional settings,

  • select the type of average voltage you want the meter to display on the summary page (Not applicable in PM5561 / PM5562 / PM5661 / PM5761 meter models),

  • change the meter passcodes,

  • enable or disable the QR code feature for accessing meter data.

See the Meter Insights QR code feature quick start guide for more information on accessing meter data using QR codes.

QR code for this page

Was this helpful?