HRB1684301-12

Harden the device

Recommendations to optimize cybersecurity in a protected environment:

  • Harden the meter according to your company policies and standards.

  • Review assumptions about protected environments and address potential risks and mitigation strategies. See Product defense-in-depth for details.

  • Terminate the user account sessions in webages.

  • Change the default passwords/passcodes. See Changing passwords/passcodes for details.

  • Change the communication protocol ports from their default values. This lowers the predictability of port use.

  • Disable communication protocol ports when they are not in use. This reduces the attack surface.

QR code for this page

Was this helpful?