Logic alarm setup parameters
Setting | Option or range | Description |
---|---|---|
Enable | Yes (checked) or No (cleared) | This enables or disables the alarm. |
Label | Logic Alarm 1 to Logic Alarm 10 (default labels) | ION Setup lets you modify the default label so it more clearly identifies your logic alarm. You can only use letters, numbers and underscores. Spaces are not allowed. |
Type | AND | Output of AND operation is True only if all inputs are True. |
NAND | Output of NAND operation is True if one or more inputs are False. | |
OR | Output of OR operation is True if one or more inputs are True. | |
NOR | Output of NOR operation is True only if all inputs are False. | |
XOR | Output of XOR operation is True if only one input is True, and all other inputs are False. | |
Priority | High, Medium, Low, None | This sets the alarm priority and notification options. |
Select Dig Output (Outputs) |
None, Digital Output D1, Digital Output D2, Digital Output D1 & D2 |
Select the digital output(s) you want to control when the alarm is triggered. |