HRB1684301-15

Meter upgrade requirements for webpages

NOTE: To know the applicable firmware upgrade method for your meter model with firmware version, refer to table Meter models, firmware versions and firmware upgrade methods.

Following pre-requisites are required for firmware upgrade:

  • Latest compatible firmware upgrade package (Download the latest firmware upgrade package from www.se.com ).

  • PC with Windows 10 and above operating system connected to meter via Ethernet network.

  • Uninterrupted power supply to the control power input of the meter, with stable Ethernet communication.

QR code for this page

Was this helpful?