HRB1684301-13

Modbus command interface

Most of the meter’s real-time and logged data, as well as basic configuration and setup of meter features, can be accessed and programmed using a Modbus command interface as published in the meter’s Modbus register list.

This is an advanced procedure that should only be performed by users with advanced knowledge of Modbus, their meter, and the power system being monitored. For further information on the Modbus command interface, contact Technical Support.

See your meter’s Modbus register list at www.se.com for the Modbus mapping information and basic instructions on command interface.

QR code for this page

Was this helpful?