Multi-state Input objects
Meter configuration multi-state input objects
Object ID | Object name | Object name / description |
---|---|---|
2016 |
Power System Type |
Power system configuration:
|
2036 |
VT Connection Type |
VT connection type:
|
3701 |
Demand Method - Power |
Power demand method:
|
3711 |
Demand Method - Current |
Current demand method:
|
3721 |
Demand Method - Input Metering |
Input metering demand method:
|
I/O multi-state input objects
The following table lists the Multi-state Input objects that provide information about meter’s I/O configuration.
Object ID | Object name | Description |
---|---|---|
7274, 7298, 7322, 7346 |
Digital Input 1 Mode Digital Input 2 Mode Digital Input 3 Mode* Digital Input 4 Mode* |
Digital input control mode
|
9673, 9681 |
Digital Output Mode 1 Digital Output Mode 2 |
Digital output control mode
|
*Available in specific meter models. Refer to Features differentiation matrix for PM5500 / PM5600 / PM5700 series for the availability. |