7EN12-0294-00

Power factor register changes

New power factor registers have been added to the meter.

The new registers provide power factor in IEC and lead/lag format, in both Float32 and INT16 data types, to facilitate importing power factor information from the meter into third-party software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?