Meter upgrade requirements for firmware upgrade tool
Following pre-requisites are required for firmware upgrade:
-
Latest compatible firmware upgrade package (Download the latest firmware upgrade package from www.se.com ).
-
Latest firmware upgrade tool which is included in firmware upgrade package.
CAUTION POTENTIAL FOR PRODUCT DAMAGE AND IRRECOVERABLEAlways use the firmware upgrade tool version which is available with the compatible firmware upgrade package.Failure to follow these instructions may result in product being damaged and irrecoverable. -
PC with Windows 10 and above operating system connected to meter via Ethernet cable.
-
Uninterrupted power supply to the control power input of the meter, with stable Ethernet communication.
-
Meters configured with STATIC IP under Stored method.
-
ION Setup configuration tool.