HRB1684301-16

Revenue-locking summary

You must configure and revenue lock your meter before installing it.
  • Unlock your revenue meter if it is locked.

  • Configure the required revenue settings specific for installation.

    NOTE: If you are using ION Setup to configure your meter, allow for any communication delays before removing power to your meter.

  • Verify the revenue settings have been implemented.

  • Clear all accumulated meter data.

  • Revenue lock your meter.

  • Verify the meter is revenue-locked.

  • Install the meter and install the terminal covers according to your meter’s installation sheet.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?