HRB1684301-13

Setting up custom alarms using ION Setup

Use ION Setup to configure custom (Cust1s) alarms.
  1. Select the custom alarm you want to set up, then click Enable to display the available setup options.
  2. Use the dropdown list to select the parameter you want to set for your custom alarm.
  3. Use the Label box to define a name for your custom alarm.
  4. Use the dropdown list to select the setpoint condition you want to monitor:
    • Over: Alarm condition occurs when the value goes above the pickup setpoint setting.
    • Under: Alarm condition occurs when the value goes below the pickup setpoint setting.
    • Over (absolute): Alarm condition occurs when the absolute value goes above the pickup setpoint setting.
    • Under (absolute): Alarm condition occurs when the absolute value goes below the pickup setpoint setting.
  5. Configure the rest of the alarm setup parameters.
  6. Click OK then Send to save your changes to the meter
QR code for this page

Was this helpful?