HRB1684301-16

THD% calculations

THD% is a quick measure of the total distortion present in a waveform and is the ratio of harmonic content (HC) to the fundamental harmonic (H1).

By default, the meter uses the following equation to calculate THD%:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?