HRB1684301-12

Unary alarm setup parameters

Configure the unary alarm setup parameters as required.

ION Setup controls are shown in parentheses.

Setting Option or range Description
Enable Yes (checked) or No (cleared) This enables or disables the alarm.
Priority High, Medium, Low, None This sets the alarm priority and notification options.
Select Dig Output (Outputs)

None

Digital Output D1

Digital Output D2

Digital Output D1 & D2

Select the digital output(s) you want to control when the alarm is triggered.
Behaviour

Normal

Timed

Coil Hold

Select the required behaviour mode

NOTE: When you select Normal value, Digital Output is not triggered

QR code for this page

Was this helpful?