IEC 61850 GGIO Onb Module
Module icon
Overview
It maps the appropriate ION values to the IEC 61850 counterparts. The GGIO_Onb Logical Node provides status information for the 8 onboard digital inputs and control capability or status information for the 7 onboard digital outputs, and can be used for IEC 61850 digital output control. Only one instance of this module can exist. Because this module is specific to supporting the IEC 61850 protocol, it can be deleted if IEC 61850 is not required.
For more information about IEC 61850, please refer to the IEC 61850 and ION Technology protocol document.
Inputs
The GGIO Onboard I/O module inputs are designed to be connected to the outputs of the Digital Input modules and the Digital Output modules.
These registers must be connected to the State outputs of the Digital Output modules for the meter’s onboard digital outputs if the corresponding Control Mode setup register is set to ion input.
These registers must not be connected if the corresponding Control Mode setup register is set to iec 61850 ctlval. Refer to “Detailed Module Operation” for more information.
These registers are connected to the State outputs of the Digital Input modules for the meter’s onboard digital inputs), which reflect the current debounced state of the digital input.
Setup registers
This register determines the source of the SPCSO1.stVal - SPCSO7.stVal output register values as follows:
-
If Control Mode is set to ion input, the corresponding SPCSO.ctVal output register value is taken from the Digital Output Status input register.
-
If Control Mode is set to iec 61850 ctlval, the corresponding SPCSO.ctVal output register value is taken from IEC 61850.
Refer to “Detailed Module Operation” for more information.
Output registers
These registers are formatted and named according to IEC 61850 protocol standards.
These registers are the status of onboard digital outputs, either taken from the Digital Output Status input register or from IEC 61850, depending on the corresponding Control Mode setup register value. Refer to “Detailed Module Operation” for more information.
These registers are the status of the onboard digital inputs, taken from the Digital Input 1-8 registers.
Events produced by the module are recorded in the Event register. Possible events and their associated priority numbers are shown in the following table.
Event priority group | Priority | Description |
---|---|---|
Reset | 5 | A module reset has occurred. |
Setup Change | 10 | Input links, setup registers or labels have changed. |
Information | 25 | not available input caused output to go not available. |
The Event output register stores the following information for each ION event: time stamp, priority, cause, effect, and any values or conditions associated with the cause and effect.
Detailed module operation
The GGIO Onboard I/O module allows IEC 61850 to control the meter’s Digital Output modules, or to read the status of the meter’s Digital Output modules, depending on the SPCSO Control Mode setup register value.
Digital Output module control through IEC 61850
![]() |
---|
unexpected digital output state change
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
If the SPCSO Control Mode setup register is set to iec 61850 ctlval, the associated IEC 61850 control attribute (ctlval) is taken from IEC 61850 and written to the corresponding SPCSO.stVal output register. The SPCSO.stVal output register is connected to the Source input register on the Digital Output module, which controls the state of the meter’s digital output. The associated Digital Output Status input must not be linked, or else the module will not go online.
Digital Output module status to IEC 61850
If the SPCSO Control Mode setup register is set to ion input, the Digital Output Status input register is connected to the Digital Output module’s State output register. The SPCSO.stVal output register is taken from the associated Digital Output Status input register value. The Digital Output status is read by IEC 61850.