Responder is a GIS hosted, distributed Outage Management System (OMS). Responder focuses on providing the most valuable information to the right people for storm restoration as well as during daily operations, allowing them to make informed decisions. Its user-friendly interface and intuitive menus allow dispatchers to perform their tasks quickly and efficiently, thus restoring power as fast as possible and making concise choices on where to dispatch crews for maximum impact based on both geographical and tabular data.

April 2019

QR code for this page

Was this helpful?