Product environmental profile (PEP)
LCA:
Life-cycle assessment ISO 14040
It includes all stages, i.e. manufacture, distribution, use and end of life, with set usage assumptions:
-
use over 20 years at a percent load of 80 % for 14 hours per day and 20 % for ten hours
-
according to the European electrical-energy model.
It provides the information presented below.
-
Materials making up the product: composition and proportions, with a check to make sure no substances forbidden by the RoHS directive are included.
-
Manufacture: on Schneider Electric production sites that have set up an environmental management system certified ISO 14001.
-
Distribution: packaging in compliance with the 94/62/EC packaging directive (optimised volumes and weights) and optimised distribution flows via local centres.
-
Use: no aspects requiring special precautions for use. Power lost through Joule effect in Watts (W) must be < 0.02 % of total power flowing through the circuit breaker. Based on the above assumptions, annual consumption from 95 to 200 kWh.
-
End of life: products dismantled or crushed. For PowerPact circuit breakers, 81 % of materials can be recycled using standard recycling techniques. Less than 2 % of total weight requires special recycling.