DOCA0176EN-02

Firmware Version 001.001.015

New Features

  • The Service Interface can be used for testing and configuring the MicroLogic 5.2 B and 5.3 B trip units mounted in the following low voltage circuit breakers:

    • ComPacT NSX circuit breakers

    • PowerPact H-, J-, and L-frame circuit breakers

    The following tests can be performed through the Service Interface:

    • Automatic trip curve test with pre-configured test points

    • Automatic trip curve test with custom test points

  • The Service Interface can be used for configuring the MicroLogic 5 A/E, 6 A/E, and 7 E trip units mounted in the following low voltage circuit breakers:

    • ComPacT NSX circuit breakers

    • PowerPact H-, J-, and L-frame circuit breakers

QR code for this page

Was this helpful?