DOCA0176EN-02

Overview

The Service Interface is a portable instrument designed for field testing. The Service Interface with part number LV485500 is used for testing and configuration of MicroLogic trip units mounted in the following low voltage circuit breakers:

  • MasterPact™ NT/NW circuit breakers

  • EasyPact™ MVS circuit breakers

  • ComPacT™ NS circuit breakers

  • PowerPacT P- and R- frame circuit breakers

  • ComPacT™ NSX circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

NOTE:
  • The information related to the new generation of ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers in this guide applies to the existing range ComPact NSX and PowerPact H-, J-, and L-frame circuit breakers also. The exceptions are mentioned wherever applicable.

  • The information related to the new generation of ComPacT NS and PowerPacT P- and R-frame circuit breakers in this guide applies to the existing range ComPact NS and PowerPact P- and R-frame circuit breakers also. The exceptions are mentioned wherever applicable.

  • These new ranges are based on the same technical and dimensional architecture as that of the exiting range of circuit breakers.

EcoStruxure Power Commission (EPC) is a global software with test functions features for testing the circuit breakers and communication accessories through the Service Interface.

QR code for this page

Was this helpful?