DOCA0176EN-06

Firmware Version 001.001.008

Bugs Fixed

During automatic trip curve test on MicroLogic trip unit:

  • Trip did not occur on the circuit breaker due to injection time out.

  • Trip occurred but the trip time was not displayed properly.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?