DOCA0224EN-00

Release History

The following table provides the summary of each TeSys island firmware package and bus coupler version:

Date

SEDP package version

Bus coupler version

Notes

September 2021

TeSysisland_002.300.006.sedp

002.300

Release with Dahlander and few security improvements.

May 2020

TeSysisland_002.200.008.sedp

02.0200

Release with extended local control modes and their integration into EcoStruxure Machine Expert software.

February 2020

TeSysisland_002.100.016.sedp

02.0100

Patch of firmware version 2.1.0.13 with Achilles certification.

January 2020

TeSysisland_002.100.013.sedp

02.0100

Release of PROFINET and PROFIBUS communication and new avatars. The firmware version is not compatible with EcoStruxure Machine Expert library.

June 2019

TeSysisland_001.100.013.sedp

01.0100

Initial release

Bus Coupler Firmware

The bus coupler firmware can be updated on the following TeSys island bus couplers:

  • TPRBCEIP (Ethernet IP/Modbus TCP)

  • TPRBCPFN (PROFINET)

  • TPRBCPFB (PROFIBUS-DP)

QR code for this page

Was this helpful?