DOCA0224EN-04

Compatibility

@Updated D1

The following table shows the compatibility of digital tools with TeSys island module in active releases.

Configuration/Programming software

TeSys island firmware version

TeSysisland_001.100.0013.sedp

TeSysisland_002.100.016.sedp

TeSysisland_002.200.008.sedp

TeSysisland_002.300.006.sedp

TeSysisland_003.000.001.sedp

TeSysisland_003.000.002.sedp

TeSysisland_003.001.001.sedp

TeSysisland_003.002.000.sedp

DTM (SoMove or any FDT container)

DTM v1.0.1401

X

X

X

X

X

X

X

DTM v1.1.0

X

X

X

X

X

X

X

DTM v2.1.1

X

X

X

X

X

X

NOTE: DTM v2.1.1 is compatible when using Modbus TCP or EtherNet/IP and for previously existing device and load avatars only.

DTM v2.2.0 or DTM v2.2.1 (equivalent)

X

X

X

X

X

X

DTM v2.3.0

X

X

X

X

X

X

X

DTM v2.4.0

X

X

X

X

X

X

X

DTM v2.4.1

X

X

X

X

X

X

DTM v2.4.2

X

X

X

X

X

X

DTM v2.4.3

X

X

X

X

X

X

X

EcoStruxure Machine Expert

EcoStruxure Machine Expert v1.1 or v1.2

Function block library: 1.0.15.0

Device description:

  • Modbus TCP : 1.1.0.0

  • Ethernet/IP : 1.1.0.0

X

X

X

X

X

X

X

EcoStruxure Machine Expert v1.2.3 or later

Function block library: 2.0.2.0

Device description:

  • Modbus TCP : 1.1.6

  • Ethernet/IP : 1.1.7

X

X

**

**

**

X

NOTE: **EcoStruxure Machine Expert is not compatible, if there is change in the IO PORT ASSIGNMENT .
NOTE: **Function blocks library for PLCs with Machine Expert on Modbus TCP protocol is not compatible.

Workaround: Use the Schneider Electric Machine Expert Modbus TCP PLCs as a third party PLC.

EcoStruxure Control Expert V15.3 SP1 or later

TeSys island Library 2021

PSx DTM Library version: 3.14.54

PLC M580 - CPU firmware 3.20

X

X

*

*

*

*

NOTE: *EcoStruxure Control Expert is not compatible, if there is change in the IO PORT ASSIGNMENT .
NOTE: If the data set length of avatars exceeds 240 bytes, then the control expert function block will not communicate with the TeSys island .

Studio 5000 V30 or later

NA

NA

NA

NA

NA

*

*

*

*

NOTE: Ensure that the export of L5X file is done with the compatible version of DTM.
NOTE: *When PIM with IO avatar is used with TeSys island , then the function blocks are not compatible with RS5000.

TIA Portal V15 or later

Library: TeSysisland_TIAV15_V2.1.1.zal15

GSD: SCHE1135.GSD (revision 1.0)

GSDML: GSDML-V2.35-SchneiderElectric-TeSysisland-20200202.xml

NOTE: Ensure that the export of AML file is done with the compatible version of DTM.

X

X

X

X

X

X

X

Library: TeSysIsland_TIAV15_V2.2.0.zal15

GSD: SCHE1135.GSD (revision 2.0)

GSDML: GSDML-V2.35-SchneiderElectric-TeSysisland-20200404.xml

NOTE: Ensure that the export of AML file is done with the compatible version of DTM.

X

X

*

*

*

*

NOTE: *When PIM with IO avatar is used with TeSys island , then the function blocks are not compatible with TIA portal.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?