DOCA0224EN-04

Firmware Update Policy

Firmware update is recommended to benefit from the latest features and potential bug fixes. It is recommended not to update the firmware to the latest version, if the latest features are not required for your application and no bug fixes are provided.

Use this release note to determine whether an update to the latest version of the TeSys island firmware is relevant for your application.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?