DOCA0224EN-02

Firmware Release History

The following table provides the summary of each TeSys island firmware package and bus coupler version:

Date

SEDP package version

Bus coupler version

Notes

August 2023

TeSys island _003.001.001.sedp

003.001.001

Korean language support.

June 2023

TeSys island _003.000.002.sedp

003.000.002

Power Interface with IO avatar is enabled for IO Optimization.

February 2023

TeSys island _003.000.001.sedp

003.000.001

Following features are updated:

  • IO Optimization

  • Local control for safe category avatars

  • Local Trip Reset for individual avatars

September 2021

TeSys island _002.300.006.sedp

002.300

Release with Dahlander and few security improvements.

May 2020

TeSys island _002.200.008.sedp

02.0200

Release with extended local control modes and their integration into EcoStruxure Machine Expert software.

February 2020

TeSys island _002.100.016.sedp

02.0100

Patch of firmware version 2.1.0.13 with Achilles certification.

January 2020

TeSys island _002.100.013.sedp

02.0100

Release of PROFINET and PROFIBUS-DP communication and new avatars. The firmware version is not compatible with EcoStruxure Machine Expert library.

June 2019

TeSys island _001.100.013.sedp

01.0100

Initial release

Bus Coupler Firmware

The bus coupler firmware can be updated on the following TeSys island bus couplers:

  • TPRBCEIP ( Ethernet/IP or Modbus TCP )

  • TPRBCPFN (PROFINET)

  • TPRBCPFB (PROFIBUS-DP)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?