DOCA0224EN-06

Configuration Software

The below are the compatible software and DTM library required to configure and use the TeSys island module:

  • SoMove software v2.9.7 or later

  • EcoStruxure Control Expert v15.0 SP1 or later

  • TeSys island DTM Library v2.4.4

  • EcoStruxure Machine Expert v1.1 or later

  • TIA portal v15 or later

  • RS5000 v30 or later

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?