Firmware Release History
The following table provides the summary of each TeSys island firmware package and bus coupler version:
Date |
SEDP package version |
Bus coupler version |
Notes |
---|---|---|---|
April 2024 |
TeSys island_003.002.000.sedp |
003.002.000 |
Following features are updated:
|
August 2023 |
TeSys island_003.001.001.sedp |
003.001.001 |
Korean language support. |
June 2023 |
TeSys island_003.000.002.sedp |
003.000.002 |
Power Interface with IO avatar is enabled for IO Optimization. |
February 2023 |
TeSys island_003.000.001.sedp |
003.000.001 |
Following features are updated:
|
September 2021 |
TeSys island_002.300.006.sedp |
002.300 |
Release with Dahlander and few security improvements. |
May 2020 |
TeSys island_002.200.008.sedp |
02.0200 |
Release with extended local control modes and their integration into EcoStruxure Machine Expert software. |
February 2020 |
TeSys island_002.100.016.sedp |
02.0100 |
Patch of firmware version 2.1.0.13 with Achilles certification. |
January 2020 |
TeSys island_002.100.013.sedp |
02.0100 |
Release of PROFINET and PROFIBUS-DP communication and new avatars. The firmware version is not compatible with EcoStruxure Machine Expert library. |
June 2019 |
TeSys island_001.100.013.sedp |
01.0100 |
Initial release |
Bus Coupler Firmware
The bus coupler firmware can be updated on the following TeSys island bus couplers:
-
TPRBCEIP (Ethernet/IP or Modbus TCP)
-
TPRBCPFN (PROFINET)
-
TPRBCPFB (PROFIBUS-DP)