DOCA0224EN-06

Version 003.001.001

New Features

Korean language support.

KC (Korean Certification) will be applicable to the below commercial references:

In scope

TPRBCEIP

Ethernet/IP bus coupler

TPRBCPFN

PROFINET bus coupler

TPRDG4X2

Digital I/O module

TPRST009

9 A standard starter

TPRST025

25 A standard starter

TPRST038

38 A standard starter

TPRST065

65 A standard starter

TPRST080

80 A standard starter

TPRVM001

Voltage interface module

TPRAN2X1

Analog I/O module

Out of scope

TPRBCPFB

PROFIBUS bus coupler

TPRPM009

9 A Power inteface module

TPRPM038

38 A Power inteface module

TPRPM080

80 A Power inteface module

TPRSM001

SIL interface module

TPRSS009

9 A SIL starter

TPRSS025

25 A SIL starter

TPRSS038

38 A SIL starter

TPRSS065

65 A SIL starter

TPRSS080

80 A SIL starter

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?