Version 002.300.006
New Features
-
Dahlander control mode is added when Dahlander Control Enabled is selected as Yes.
-
Certificate Manager is added to configure the security certificate to the TeSys island module.
-
Cybersecurity improvements.
-
When bus coupler is in fallback IP, there will be no duplicate IP address check.
Bugs Fixed
-
Transition between states did not reset avatar logic inputs.
-
Dynamic Host Configuration Protocol (DHCP) caused major fault or failure in Ethernet service if routed through another TeSys island module.
-
Bus coupler did not go into power failure mode when powered by 12 V signal.
-
Voltage asset information from Voltage Interface Module (VIM) had incorrect scaling.
-
DTM accessories were not correct for size three starters (displayed the size of 1 kits).
-
Total active power and total reactive power for system avatar include avatars without Energy Monitoring Enabled.
-
Detected frequency based on the A-C voltage instead of A-N voltage when configured for single-phase.
Known Issues
-
Local mode status has not worked for Conveyor One Direction - SIL Stop, W. Cat 1/2 and Conveyor Two Directions - SIL Stop, W. Cat 1/2.
-
Load from Device does not work when there are more than 16 SIL starters in the configuration.
This issue exists in all the previous TeSys island firmware packages.
Workaround: Save the configurations in SoMove or EcoStruxure Machine Expert software and connect to the device without using Load from Device.