DOCA0224EN-07

Version 003.003.000

@New D1

New Features

IO Optimization feature extension to EcoStruxure Control Expert function blocks library.

Bugs Fixed

  • Incorrect asset data (running hours) is displayed in SoMove and Operation and maintenance tool after firmware upgrade.

  • When a firmware upgrade or downgrade occurs, the correct firmware version information is not updated in the audit log.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?