Utility-Generator Operation

  1. Detect the normal source contingency (Utility).
  2. Send out Genset start signal when normal source is out of tolerance.
  3. Transfer the load to replace source (generator) when generator is ready.
  4. Re-transfer to normal alternate source when it is recovered if auto return mode is set.
  5. Send the Genset cool down signal after re-transfer to normal source.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?