Library File String Variables for novA Offer

MasterPact MTZ and NT/NW

MasterPact

MasterPact NT/NW

MasterPacT MTZ

MasterPact MTZ1

MasterPact MTZ2/MTZ3

MicroLogic

MicroLogic

MicroLogic X

Software

The following variable Ecoreach_software tracks the name change of Ecoreach to EcoStruxure Power Commission in November 2018.

EcoStruxure Power Commission

Units: (01/2018) in EN, FR, ES: phase names are NoTrans. In Chinese: translate phase names in Variant country:International must be the phase name in Variant country:USA (that is, 1-->A, 2-->B, 3-->B in Variant country:International

Variant information:

  • country

    International

1

Variant information:

  • country

    International

2

Variant information:

  • country

    International

3

VEGA offer (PSE461.4, PSE747.3)

ComPact NSX

Variant information:

  • country

    International

ComPact NS

Devices

EIFE

“IFE_EIFE” variable used in PSE695 (IFE guide) and PSE1288 (EIFE guide) to distinguish the product’s specificity.

“IFE-EIFE_byCBtype” variable used in Modbus communication guide (PS1054 MTZ, PSE747 Compact NSX, PSE461 NT/NW) to distinguish the Ethernet interface used depending on the Circuit Breaker type.

Variant information:

  • cbtype

    NSXm

IFE

Mobile Power Pack = name of a power supply module

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?