DUG_Wiser_Airzone_WH-02

About Airzone Plenum and Wiser System

IMPORTANT: Airzone is applicable for customers in France, Portugal, Spain and United Kingdom.

Airzone plenum is a zoning system used with ducted air conditioning systems, to manage the temperature of each zone of a house. The air conditioning system adjusts the air temperature and circulates it in the house, ensuring a comfortable indoor environment.
The Airzone plenum is connected to the heat pump allowing you to set different temperature set points for different zones of the house. This makes the use of energy only in the occupied zones, thus reducing the cost of system operation.
Using the Wiser Home app, Airzone plenum system is connected to a Wiser Hub via Wi-Fi®. Then the temperature in each room of the home can be regulated with the Wiser Home app.


Features:

  • Provides the temperature readings in the Wiser Home app.

  • Allows to control the set points and various operating modes of the system.

  • Provides the ease to schedule the heating and cooling of multiple rooms with the Wiser Home app.

  • Optimizes energy consumption by adding a window/door sensor or a motion sensor per room.

For more information on Wiser, please refer to Wiser System - France, Wiser System - Spain and Portugal or Wiser System - United Kingdom as per your country.

Advantages:

  • Wiser Home app acts as the single interface for managing the multiple Airzone devices.

  • Wiser system enhances the energy management capabilities.
    For example, it optimizes an AC according to energy tariffs and makes the best use of energy produced by the photovoltaic (PV) panels.

About Aidoo Pro Wi-Fi® for air conditioner

IMPORTANT: Aidoo Pro Wi-Fi® is applicable for customers in France, Portugal, Spain and United Kingdom.

Aidoo Pro Wi-Fi® (hereafter referred to as Aidoo) is a solution that lets you control individual air conditioner (AC) through the Wiser Home app. An Aidoo is wired to the AC internal unit and connects to the Wiser Home app via Wi-Fi.
You can control multiple ACs using the Wiser Home app.
Advantages of Aidoo:

  • Remote control of the AC through Wiser Home app.

  • The wired connection between Aidoo and the AC ensures:

    • reliability in controlling the AC,

    • zero communication failures and unintended activations.

  • It maintains the inverter functionality and efficiency levels of the AC.

  • Aidoo can communicate with the AC internal unit using the manufacturer’s protocol.

    NOTE: Each Aidoo is compatible with a single AC manufacturer. Depending on the AC brand and model, the installer must choose the right Aidoo.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?