DUG_Wiser_Airzone_WH-02

Operating modes

Using the Wiser Home app, you can manage the operating modes for Airzone devices.
  1. On the Home page, tap All devices > Airzone device.
  2. On the device control panel page, tap (A).
    The operating modes will be shown (B) automatically according to the connected Airzone device.

  3. Select any one of the available modes (B) and drag the sliding bar up/down (C) to adjust the set-point temperature (Heating, Cooling and Dry):
    • Heating

    • Cooling

    • Dry

    • Ventilation

    • Stop

    Room settings: You can edit the room name for the device.

    The current operating mode indicates the mode in which the system is working.
    • Off : Turns the system off.
    • Heating : System operates in heating mode when the set-point temp > room temp.
    • Cooling : System operates in cooling mode when the set-point temp < room temp.
    • Dry : System operates in dry mode, reducing the humidity and refreshing the environment when set-point temp < room temp.
    • Ventilation : System operates in fan mode when set-point temp < room temp.
    • Stop : When the set-point temperature has reached, the AC unit remains switched on in low consumption mode (Stand-by mode).
    • Boost mode: Boost Mode will apply a boost of +2 °C for one hour to every room in the system. For more information on different modes, refer to Wiser Modes.
    • Auto mode :(This mode is available only for Aidoo) Enables automatic switching between cooling and heating and can turn off when required.
      IMPORTANT: Auto mode can be activated only via the Airzone app.
    NOTE: To access live, history and energy insights, it’s recommended to install PowerTag on the Airzone loads. Refer to Checking device consumption.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?