DUG_Wiser_Airzone_WH-02

Creating a moment

To create a moment:
  1. On the Home page, tap > Moments > .
  2. Enter the name of the moment (A).
  3. Tap Add actions (B) to select the list of devices.
  4. Select the devices (C) you want to set an action and tap Done.
  5. On the Moment creator page, select any one of the following device (D) and set actions.
  6. Drag the sliding bar up/down (G) to adjust the temperature as per need and tap Set.
  7. Once all conditions are set, tap Save.
    The saved moment is shown on the Moments tab. You can tap on the moment to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?