DUG_Wiser_Airzone_WH-02

Creating a schedule

The Airzone system can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule for Heating and Cooling. You can create or modify the schedules at any time.

To create a schedule:

  1. On the Home page, tap > Schedules >

    Once the Airzone devices are installed and paired with the Wiser Hub, user gets notified in the Schedule tab.

  2. Read the tutorial information and swipe to navigate to next screen.

    NOTE: There is a pre-defined schedule for your Airzone devices. You can follow the same or change the schedule as per need.

    New Schedule page appears on the app screen.

  3. Enter a name of the schedule (A).

    NOTE: TYPE is Climate by default, you cannot change it.
  4. Select the type of temperature control (B).

    NOTE:
    • You can see only the Temperature control part that you have installed. Example, if you have installed only the heating system, you cannot view the cooling temperature control

    • You should select Heating and Cooling as the temperature control option for air conditioning systems.

    .
  5. Select the list of devices (C) to which the schedule must apply.

  6. Tap Create > See my schedule.

  7. Tap to add an event.

  8. Select a temperature (D), time period (E) and tap Set.

    TIP:
    • You can add multiple schedules based on your requirement. Select days, tap , set temperature and time.

    • You can copy the existing schedule to another schedule or to the days of your choice. Tap .

      • Tap Schedule and select an existing schedule and tap Copy.

      • Tap Day and select the days you want to assign and tap Copy.

      NOTE:
      • If the boost mode is turned on and in this period if there are one or more scheduled actions (Heating or Cooling), the system stops the schedule action temporarily and only performs the boost operation until the boost duration is completed.

      • If you adjust a setpoint from the control screen and there are one or more schedules actions set. The scheduled setpoint is overridden and the room follows the manual setpoint until the next scheduled event.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?