DUG_Wiser_Airzone_WH-02

Setting the device location

You can change the device location using Wiser Home app (such as bedroom, living room, dining room etc.).
  1. On the Home page, tap .
  2. Tap Devices, select the device from the list for which you wish to change the location.
  3. Tap Location to open the device setup page.
  4. On Device Setup page, you can enter New room name (A) or select an existing room from the list (B).
    TIP:
    • If the device is already assigned, you can remove it from the existing room. Tap Remove from Room (C).

    • If Airzone and other heating/cooling devices are in the same room, it is recommended to assign one of them to another room using the Wiser Home app. Example, if you have a heating device such as Wiser room thermostat in the same room where Airzone is installed for cooling, remove any one of the devices in the app and assign it to a different room.

  5. Once changes are done, tap Submit (D).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?