DUG_Wiser_Airzone_WH-05

Away Mode

Away mode allows you to configure your devices even when you are away from home. For example, you can set the temperature and turn on/off the devices as necessary. Refer to Away Mode - France, Away Mode - UK or Away Mode - Spain and Portugal for detailed information as per your country.

  1. On the Home screen, tap > Away Mode > HVAC .

  2. Select the mode which you want to activate/deactivate in away mode.

  3. Tap .

    NOTE: Tap Reset to restore the default mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?