DUG_Mureva EVlink_Socket_WH-03

Enabling Reduce My Bill with AI

The following is an example of enabling RMB-AI with EV Charger and Water heater installed.

To enable RMB AI:

  1. On the Home page, tap Energy Dashboard > Insights, then tap splash screen (A).

  2. Tap (B) to read the tutorial information.

  3. Follow any one of the steps as per need:

    • Tap (C) if you want to use the basic offer.

      NOTE: Basic offer is the RMB - Expert rule offer that is already opted.

      • A notification window will be prompted for confirmation. Tap Continue. Refer to Reduce My Bill

    • Tap (D) if you want to use the RMB-AI offer.

    • On the Home Profile page, tap Continue.

  4. Set the time when you want your car to be charged:

    1. Tap (E), select a time period (F) and tap Set.

    2. Tap (G), select a time period (F) and tap Set.

  5. Tap Next.

  6. Enter the number of kilometers required to drive this car using the dial pad:

    1. Tap On week day

    2. Tap Over the entire weekend

    NOTE:
    • If you have any one of the supported devices commissioned, you will see only the related questions.

    • If you have all the supported devices commissioned, you will see all questions related to the devices. Example, if you have both EV Charger and Water Heater, you will see further questions for Water Heater.

  7. Tap Next.

  8. Enter how many members take showers using the dial pad:

    1. Tap In the mornings

    2. Tap In the evenings

  9. Tap Next.

    You will be directed to Insights tab.

Enrolling additional devices

You can add additional devices of different types to RMB-AI. For instance, if you have enrolled 1 EV Charger and 1 Water Heater and you wish to add another EV Charger or Water heater. You must disable the previously enrolled device to enable the new device (EV Charger or Water Heater).


The following is an example of enrolling additional EV Charger or Water Heater with the same type of the existing device.

  1. On the Home page, tap > Energy Management > Reduce My Bill.

  2. Tap EV Charger (A) or Water Heater (B).

    A notification window will be prompted. Read the information.

    1. Tap OK to close the window.

  3. Disable the first enrolled device to enable your additional device.

    A notification window will be prompted that Removing the Reduce my Bill schedule mode may impact your cost savings and will revert to customised schedule if present or manual mode.

    1. Tap Continue.

  4. Enable the toggle switch (A) or (B) of the new device.

NOTE: After enrolling devices to RMB-AI, refer to Using Reduce My Bill to view how the devices are controlled and scheduled for usage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?