DUG_Mureva EVlink_Socket_WH-03

Setting Tariff

You can set tariff in the Wiser Home app to access your energy cost and billing data.

You can set the tariff based on your contract type:

  • Flat rate: Flat rate is defined as the fixed rate for the entire time period of electricity service. Configuring - flat rate.

    Peak/Off-Peak Hours rate: Peak rate is defined as a rate set to a specific period of time at which electrical consumption is at its highest. Off peak rate is the time period when the demand for power is at its lowest. It is the amount you pay for each unit of electricity consumed for the time period set. Refer to Configuring - peak rate.

  • No contract: Electricity rate is not set, no information related to bill will be shown in the app.

    NOTE:

Once the device is commissioned, user gets notified that this feature is available. The Tariff Entry screen appears on the Home page.

  1. Tap Continue.

  2. Read the feature update and swipe to navigate to next screen.

  3. Tap to close the overlay screen.

    NOTE: If you have not configured your tariff, a push notification will be sent after 2 weeks and the last reminder after 6 weeks.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?