Configuring - flat rate
- After reading the Tariff onboarding information. On the Tariff screen, tap Electricity.NOTE: If you have already configured your tariff settings, follow below menu navigation if you need to modify tariff rate
On the Home page, tap . - Tap (A) and select Flat.
- Tap (B) to set the contract limit.
The Contract Limit page appears.- Select your contract limit (kVA/A/kW) from the dropdown
menu, then tap and enter a value using the
dial pad as per your country.NOTE: Contract limit is the maximum permissible power on the Grid on your contract. It will help to prevent power tripping by shutting down loads in order to keep the power consumption under a defined limit. By default, the contract limit is set to measure in kVA.
The following table displays the default values within the range:
Country
Default Value
Range
France
36 kVA
1–42 kVA
Germany
60 A
15–160 A
Spain
15 kW
1–42 kW
Belgium
40 A
15–160 A
Sweden
20 A
16–63 A
Denmark
25 A
25–35 A
IMPORTANT: You cannot enter a value that is greater or less than the specified range.A notification window will be prompted that the Contract Limit is used by Anti-Tripping Management algorithm. If set incorrectly it may not work as expected and could result in the power tripping.
IMPORTANT: Anti-Tripping is applicable only if you have installed Water Heater/EV Socket/Schneider Charge/EVlink Home Smart in your home.For more details, refer to Anti-Tripping (Add Link). - Tap Continue, if you like to proceed.
- Select your contract limit (kVA/A/kW) from the dropdown
menu, then tap and enter a value using the
dial pad as per your country.
- Tap (C) and select a subscription type (D) (refers to recurrent fee).
- Enter a value in the Cost (€) (E) field and tap Set.
- Tap (F), enter a flat rate of consumption in the Rate - €/kWh field and tap Update.
- Tap Save (G).