Configuring - (peak/off-peak) rate
- After reading the Tariff onboarding information. On the Tariff screen, tap Electricity.
- Tap (A) and select Time of use (peak /off-peak hours).
- Tap (B) to set the contract limit.
- Select your contract limit (kVA/A/kW) from the dropdown
menu, then tap and enter a value using the
dial pad as per your country.NOTE: Contract limit is the maximum permissible power on the Grid on your contract. It will help to prevent power tripping by shutting down loads in order to keep the power consumption under a defined limit. By default, the contract limit is set to measure in kVA.
The following table displays the default values within the range:
Country
Default Value
Range
France
36 kVA
1–42 kVA
Germany
60 A
15–160 A
Spain
15 kW
1–42 kW
Belgium
40 A
15–160 A
Sweden
20 A
16–63 A
Denmark
25 A
25–35 A
IMPORTANT: You cannot enter a value that is greater or less than the specified range.A notification window will be prompted that the Contract Limit is used by Anti-Tripping Management algorithm. If set incorrectly it may not work as expected and could result in the power tripping.
IMPORTANT: Anti-Tripping is applicable only if you have installed Water Heater/EV Socket/Schneider Charge/EVlink Home Smart in your home.For more details, refer to Anti-Tripping (Add Link). - Tap Continue, if you like to proceed.
- Select your contract limit (kVA/A/kW) from the dropdown
menu, then tap and enter a value using the
dial pad as per your country.
- Tap (C) and select a Fixed Charges type (refers to recurrent fee) -Yearly, Monthly, Weekly, Daily.
- Enter a fixed charge value in the Cost (€) field and tap Set.NOTE: The Fixed Charges is applied to recover the basic cost of electric service, independent of how much energy is used. These charges are electricity costs that don't change no matter how much electricity you use. This amount is fixed in your electricity bills.
- Tap (D), enter peak rate of consumption in the Rate - €/kWh field and tap Update.
- Tap Add a rate.
- Enter the name of the rate in the text field (E).
- Enter a target value in the Rate - €/kWh field (F) and tap Add (G).
- Tap Add a Schedule (H) to set the time frame.
- Enter a schedule name in the NAME field. Example, Weekend tariff.
- Select the days of the week in DAYS field to apply the schedule.
- Tap to set Start time and Finish time.
- Tap and select a RATE
TYPE.IMPORTANT: It is necessary to set off-peak hours for each day per schedule (I) else you will not be able to save your tariff details.
- Tap Add and then tap Save.