DUG_Odace SSO_WH-04

About Quick Home Connect

Quick Home Connect is your starting point for wireless home automation. It performs functions like switching, dimming and shutter control using a Connected Wireless Switch (hereinafter referred to as Wireless switch) via a Zigbee network.
IMPORTANT: Applicable only for products sold as a part of Quick Home Connect kits.

Quick Home Connect is a wireless connectivity solution for Zigbee devices without the need for a Hub or smartphone application.

The Wireless switch is a battery-powered wireless push-button switch that is used to control Zigbee devices (such as light or shutter) within the same Zigbee network.

Supported devices

  • Connected Universal Rotary Dimmer (Rotary dimmer)

  • Connected Blind Control Switch (Blind control)

  • Connected Single Socket Outlet (Socket outlet)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?