DUG_Odace Rotary Dimmer_WH-03

Pairing the device in Quick Home Connect

The Wireless switch can be paired with the supported devices in the list. Refer to Supported devices.

Preparing the devices:

It is necessary to prepare the devices before pairing. On certain devices the status LED is not directly visible.

  1. Remove the rocker of the Wireless switch.

    • Make sure the Wireless switch is aligned correctly to identify the pairing buttons.

      • 1-gang wireless switch: Pairing button (A)

      • 2-gang wireless switch: Pairing button for the right channel (A)

      • 2-gang wireless switch: Pairing button for the left channel (B)

    NOTE: The Wireless switch is configured for 1-gang operation by default. To switch from 1-gang to 2-gang operation, refer to Switching from 1-gang to 2-gang.
  2. Remove the knob of the Rotary dimmer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?